Hi team,
My customer has a question on the oscillator frequency.
In the datasheet, there is a min/max value that is given at T=[-40;+85degC].
Do we have a min/max value only at 25degC?
Thanks in advance for your feedback.
Pol
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer has a question on the oscillator frequency.
In the datasheet, there is a min/max value that is given at T=[-40;+85degC].
Do we have a min/max value only at 25degC?
Thanks in advance for your feedback.
Pol
Doc2.docxHello Pol,
The frequency range for the UC2854 is not specified at 25 deg C.
However are you sure thatit is not the UC285A or UC2854B that you are interested in ?
These are newer parts with significant changes from the older UC2854.
The frequency range for these parts is specified in Figure 7 of the data sheet and attached.
It has a frequency range from about 10kHz to 800kHz
Regards
John