Hi Team,
Our customer is seeing some anomaly when sending the BQ40Z50 battery gauge into shutdown mode and having a charge voltage present during the DELAY time. Could you help provide some guidance from the observations below?
We observed that a charging voltage applied at the battery between the time after the command SHUTDOWN Mode (0x0010) was sent and the battery chip enters shutdown mode causes
an unexpected behaviour. According to the technical reference manual (bq40z50-r1 - July 2015 - page 81) it is stated that after the command is sent to the battery chip an internal counter is started.
When the counter reaches Ship FET off Time, it turns off the CHG and DSG FETs and if it reaches Ship Delay the battery chip will enter Shutdown mode.
In our case, the timings are as follows:
Ship FET off Time : 10s
Ship Delay : 20s
We tried following test sequence:
- send command to enter shutdown mode
- disconnect charger
- wait 10s- 13s - after 10s the voltage at the battery is turned off as expected
- connect charger
- wait e.g. 200ms - 1s
- disconnect charger
- wait additional 20s - expect that after wait time the battery chip is in shutdown mode.
- connect charger
- wait 5s - wake up battery chip
- disconnect charger
- check if battery is woken up
We observed the following behaviour after we ran the test sequence above:
1) wakes up automatically ~2 minutes after the command was sent to the battery chip
2) wake up works if charger is applied after ~1 minute. Before it does not wake up the battery chip
Additionally, if 1) or 2) happens, there is a chance that the battery chip does not enter shutdown mode via command for up to ~3 minutes.
We read out status registers 0x50 - 0x55 when the wake up did not work as expected.
In 0x54 OperationStatus we could see, that the flags
CHG = 0 - Charge FET inactive
DSG = 0 - Discharge FET inactive
SDM = 1 - Shutdown triggered via command active
Can you please give advice on how to avoid this state we’re ending up and how the set the chip back to normal operating mode?
Thanks for the help and best regards,
Jerry