This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMB1428Q: EMB1428Q shows intermittent failures (fault codes 0x90 and 0xB0)

Part Number: EMB1428Q

Hello,

We have a custom design based on EMB1402 evaluation board, consisting of EMB1428 and EMB1499. This is used to charge discharge a stack of 2Volt batteries. The system functions(able to charge/discharge cells), but intermittently shows failures(fault codes 0x90, 0xB0, 0x70 & 0xC0) on some of the lowside cells( near to ground of the battery stack). The chip however recovers from the fault on subsequent charge/discharge command. For example, I have summarized below two cases when I am trying to discharge the first cell(from ground) on the battery stack.

Case 1(faulting initially, however recovering when discharge command is continuously issued every 4seconds):

Time line (seconds) Command Fault code
0 discharge  0xB0
4 discharge 0xA0(no fault)
8 discharge 0xA0
12 discharge 0xA0

Case 2: (faulting every time. Discharge command issued discretely, followed with open all switches command)

Time line (seconds)  Command  Fault code
0 discharge 0xB0
                4 open all switches
                5 discharge 0xB0
8 open all switches
9 discharge 0xB0
12 open all switches

Similar behavior is observed while trying to charge the cells. The battery stack consists of 12, 2V cells. We use two EMB1428 each one driving its on EMB1499. Each EMB1428 drives 6 cells. The issue is always seen on EMB1428 connected to the lowside bank of the battery stack.

We have below questions regarding this issue.

Is this an expected behavior? If so, does the chip requires a warm up time for charging/discharging?

What is the reason for those faults(0x90, 0xB0, 0x70 and 0xC0) to show up intermittently?

Is it an indication of the part being stressed intermittently which eventually could damage it permanently?

Thanks

Brayan

  • Hi Brayan,

    Let me look into this and get back to you on Monday.

    Best regards,
    Leslie
  • Hi Brayan,

    I looked at the fault codes you mentioned and I suspect this could be related to noise in your system since one of the faults you mentioned (0x70) is not a valid fault code (see page 22, table 3 in EMB1428Q datasheet for valid fault codes). I recommend checking that your supplies look clean without overshoot, undershoot or a lot of ringing.

    Are you using TI's EM1402 EVM or your own design? If you are using your own, could you please share it to review it?

    Are you using your own software?

    Regards,
    Leslie