Other Parts Discussed in Thread: TPS65218D0, BOOSTXL-TPS65218, LM26480, TPS82085
Hello team,
I bumped into an application in a radio module in which we have 3 output supply rails 1.8, 2 and 3.3V ( Current max-1 A).
Currently in the design there is TPS62097RWKR ( 3.3V to 1.8V), TPS82085SILR ( 3.3 ---2V) and an LDO AP2156SG-13 ( with 2 output 3.3 rails). Vin is also 3.3V for the LDO.
It would be great if you could suggest me one Power module with 2 LDO outputs, 2 DC-DC outputs, so in total 4 outputs needed. I'm quite familiar with WEBENCH , but I'm not able to find what I need.
Additional info : Current rating for the loads ---worst case is 800 mA
Cost has to be kept in mind.
Do you have any suggestion?
Thanks in advance.
Best regards,
Adrian