Hi,
I am working on the calibration of RX per SLUA731 (FOD GUI User's manual), section 6.3. The equipment requires Source meter with 3-A current rating (Keithley 2425) uses as a load during the calibration.
For my application, the battery we chose has 1000mA charging current. Do you think it is sufficient to use Keithley 2400 instead, that has 20W, +/-1uV to 200VDC, +/-10pA to +/-1A specification?
Furthermore,
Since the Source meter is used as a load, to adjust the current, do I need to use current sink function? in other words, should the current be negative? Table 1 from SLUA731 shows positive current. I am a little bit confuse on this part.
Thank you for your help
-Bo