This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: Maximum output current

Part Number: LM5175
Other Parts Discussed in Thread: LM5176

Hi Guys,  The LM5175 spec indicate maximum output current 20A.  However the chip uses external FETs for the switching.  Assuming the FETs are of low gate charges, the input range is narrow (3:1), and input-output differential is small (say 20V input and 15V output), and a proper current sense resistor is chosen, what is the limiting or determining factor for the maximum output current as far as the chip is concerned?