This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM20146MHEVAL: SW waveforms

Genius 4840 points
Part Number: LM20146MHEVAL
Other Parts Discussed in Thread: LM20146

We got SW waveforms using with LM20146MHEVAL.

Condition is

Vin:5.0V,Iout:1A CR mode   EVM is default

Vin:5.4V,Iout:1A CR mode   EVM is default

Please see the point of red circle at page2 in attached file.(Vin:5.4V,Iout:1A)

Please let us know the reason why these waveform was seen at EVM.

Does this waveform cause any problem ?  

LM20146MHEVAL.pptx