This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS562200: TPS562200 is warming up or does not give the desired output.

Part Number: TPS562200

Tool/software: WEBENCH® Design Tools

Dear All,

I designed the circuit with TPS562200 that the input voltage is 5-12V and output voltage is 3.3V 1A. I used the WEBENCH Design Tools and TPS562200 datasheet.

I produced the 20 pieces prototip board and 14 boards worked properly. I'm deal with non-working boards. I disassemble processor non-working 6 boards. I noticed that  ground and 3v3 of 4 processor pins shorted.

I think the reason for this is the regulator TPS562200.

I decided to look at the output voltage of the regulators. Although I give the same voltage at the input, 1 of the regulator output 1.66V and the other 4.07 volts. The other 2 one it attracts current in a wavy manner

and gets  very hot.I checked the components wrong and tried again but the components were correct.

As a result, 1 regulator output 1.66V

1 regulator output 4.07V

2 one attracts current in wavy manner and gets very hot.

İs there someone who can help? What could have done wrong. 16 out of 20 working boards.

lg_gway_v4.0.pdf