Dear TI Team,
we are doing some tests where device pins are shorted and check the application behaviour.
On the TPS51206 we did a test and shorted Pin10 (VDD) to Pin3 (VTT). In this test the device gets very hot >>150°C and we see a risk of fire hazard.
- VDD = 5V
- VLDOIN/VDQSNS = 1.5V
- VTT = 0.75V
1) Are VTT pin or VDDQSNS pin diode clamped to VLDOIN?
2) In case yes, what is the maximum clamp current?
We consider to limit the current on VDD to avoid the themal runaway issue.
Other recommendations to overcome this issue in a pin short event are welcome.
Thanks and best regards,
Joe