Other Parts Discussed in Thread: TPS61175
Dear TI,
I am looking to use TPS61089 for 7.2V Li-Po battery charger. My question is
- Can I use the input of PC USB port to charge the Li-Po using TPS61089. The minimum current of USB is 500mA and 5V is this good enough to generate 7.2V and 1 or 2A.
- Datasheet didn't mention minimum input current only Peak Switch Current Limit, is this the actual limit?
- If this TPS61089 is not suitable, can you please recommend another IC able to produce similar current and voltage from above output.
Thank you and appreciate your help