This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568215: Maximum value of output capacitor

Part Number: TPS568215


Hi,

Looking at Table 5, Cout (max) is 500 μF.
However, the total bypass capacitors placed away from the IC will be over 500 μF.
is there a problem? Do I have to keep the total of 500 μF or less including this bypass capacitor?

Best regards,
Yuto Sakai