This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: Input 56 VDC

Part Number: LM5022
Other Parts Discussed in Thread: PMP11047

Hello,

I'm evaluating the solution proposed in the file:

tidrdz3.pdf

PMP11047_REVA.SchDoc

My costraint is an input voltage of 18 - 56 VDC, instead of the input of 18 - 48 VDC proposed by the application displayed in the file.

My question is if I can  use this schematic with the max input voltage of 56 VDC instead of 48 VDC.

Thank you.

Maurizio