Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Good seniors.
Today, I used simplis to build a half-bridge power supply simulation model based on the LM5035 controller, but I was given an error.
*** ERROR *** Cannot find DC operating point - No convergence in pseudo transient analysis.
Do you know why?
I downloaded the simulation model they made from the official website, as shown in the figure above.
However, this model can only be opened in OrCAD Capture CIS software. Since I have a trial version and there are component limits, I can only see the simulation circuit model, but I can't simulate it.
I rely on the gourd painting, and I have this half-bridge model in simplis. as follows:
I suspect that there may be a problem with the imported model of the LM5035, because I have block simulations of other circuit diagrams, although the circuit does not work properly, but no error is reported.
Simulation model that can be downloaded from the official website:
Here is the simulation model I built in simplis: