Other Parts Discussed in Thread: LM5170,
Hello,
i'm planning to use 2 LM5170 in a 4Phase configuration. Total power 3KW 12V/48V (62,5A per Phase).
My plan is to use the following MOSFET (two in parallel) IAUT300N10S5N015. Due to the massiv Cin and total gate charge i'm concerned that the internal driver of the LM5170 wont be able to support sufficient rise/fall times.Sadly i can't find the total power the gate drivers of the LM5170 are able to supply in the datasheet. Only the peak current of 4A/5A is given.
So my Question is the following:
# What is the maximum power delivery of the high and low side gate driver ?
# Can i connect an external gate driver ic to the lm5170, by using pin LO1 as signal input for external gate drive low side?
For the high side input i want to connect pin SW1/SW2 permanently to Ground, pin HB21/HB2 permanently to +10V (referenced to GND) and using pin HO1/HO2 as the input for the external gate drive high side. Is this possible?
Kind regards,
Jochen Rohm