This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2546: TPS2546 Can we shorten the detection time? Or cancel?

Expert 2630 points
Part Number: TPS2546
Other Parts Discussed in Thread: TPS2544

Our charging cabinet (TPS2546 chip for USB) has load detection function.  
When no load is detected, the USB port of the charging cabinet will not output current.  
The charging cabinet charges the flat panel for a few seconds and then disconnects for a few seconds.
This leads to low charging efficiency.This can lead to a long period of inadequate charging.
Seen from the table below          
 When there is no load, 0.2S will be disconnected.           
When there is load, 3S will not supply power until after.           
Can we shorten the detection time? Or cancel?           
Can TPS2544 be replaced?