This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5085: Current output LM5085

Part Number: LM5085

Hi!

I want to made a buck circuit with the LM5085 controller for a 42V-56V input and 12V output with 3A. However, when i want to prove the circuit i can only have 2.3A in the output, but the specification of the LM5085 say that the output can be 10A. I don't shure that i made bad, but i don't a 36W output like i'm expected. The schematic is: