Part Number: TPS2419
Dear TI,
We are currently designing a N+1 Redundant Power Supply.
With the schematic as it is, (RSet = 35 ohm) we are able to get the power supply functioning properly when both Power Supplies are connected. However if one power supply is disconnected, there will be reverse current in the MOSFET, so the current will flow from the circuit to the Power Supply(which is undesirable). We tried to increase the value of Rset (we removed the Resistor), but the issue still remains.
Is there any issue with the design or with the components we are using?
Thank you,
José