This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS40210: WEBENCH® Tools/TPS40210

Part Number: TPS40210


Tool/software: WEBENCH® Design Tools

Hello,

I build a boostcontroller with the aid of WEBENCH. I used the components that WEBENCH suggested

The specifications are :

Vin 4.5-5.5V

Vout 12V

Iout 300mA

The circuit works, but does not hold its output voltage while load increases.

What can be the cause?

Thanks