This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AUDIO recommendation?

Other Parts Discussed in Thread: TPA3111D1-Q1

Hi

AUDIO output, please help recommend the audio power amplifier chip, the main functions are as follows:           

1. The system is a 24V system, and the range of VBAT is 16-36V.           

2. The trumpet model is 4 ohms, 3W.           

3. The output pin of power amplifier needs short circuit protection for VBAT and GND. (When doing short circuit protection experiment, the voltage of VBAT is less than 30V)           

BTW, some customers use LM48100Q, can also achieve short circuit protection for VBAT and GND (12V system). This chip should not have this function.

Is it experimented through external circuits? Do you have some solution?

Thank you

Jerry