Part Number: BQ24780S
What is the Shipping Mode? When should SRN pin discharge current?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In 8.2.2.3 of datasheet, we can see that:“ Some packs may wake up again if the voltage on SRN pin stays above pack UVLO too long.”
In my opinion, battery will constantly deliver the current to system through body diode when the system is totally shutdown, so that Vsys will be pulled up, then some packs may wake up.
For this reason, we should enable the shipping mode to discharge the current of SRN. And without the current from battery, Vsys will down to 0 to minimize the quiescent current.
I don't know if I'm right.
If so, for there are only 140ms to discharge current in the shipping mode, should we enable the shipping mode frequently? Or , when we enable the shipping mode, IC will automatically discharge current when needed? And what is the threshold to discharge current.
Hi,
This charger's shipping mode function should work with battery pack's internal MOSFET. Before you enable shipping mode, you should send command to battery pack to turn off internal MOSFET to force Battery disconnect to charger. But because there still bias voltage existed in battery connector to re-force battery pack turn on again. So enable shipping mode can force BQ24780S to discharge residual voltage via SRN pin.
You don't need to enable shipping mode frequently when customer use normally. Just for product ship from your factory.
Thanks