The board has accelerometer interfaced to ADCIN0 and ADCIN2 of TPS65930. We are presently testing the ADC interface. From SWCU052A TPS65930 TRM, p403, The adcin0 pin is connected to current source by default. This has to be changed to GP mode by configuring the TYPEN and ITHEN bits of BCICTL1 register. But i could not trace these registers in the datasheet. Once the MADC is powered on byt setting the MADCON bit, the conversion is happenning and the status is observed to be Busy, also the interrupt is not coming. Pls can you clarify. The TI EVM has ADCIN interface, but in that TWL4030 is used.