Other Parts Discussed in Thread: BQ40Z50, GPCCHEM
Hello,
Regarding IATA shipment requirement, the battery SOC should be <30%.
Based on this, all batteries shipment SOC range is 25%~30%.Now we met the SOC under this range 25%~30% during IQC inspect battery in winter. Almost battery packs SOC around 18%~20%
The problem is the battery had experience a low temperature during transportation, about 5degC that make gauge calculation characteristic under low temperature.
In this case, what is the accuracy of bq40z50 at low temp 5degC?
Ju