Other Parts Discussed in Thread: PMP9446, PMP
Dear Team,
My customer want to use this reference design for Vin=12V, Vo=54V, Io=0.5A
I found some question on it:
1. The transformer turn ratio is 6:24, so the maximum Vo should be 48V right? Even Duty=100%, I still don't think 12Vin will have 54Vo.
2. For the secondary side diode, why you use 600V/10A rating?
Base on my understanding, this reference design is for 54V/0.75A output. So diode reverse voltage should be 12*4+54=102. Diode average current should be 0.75A.
BR
Kevin