Other Parts Discussed in Thread: UCC27712
Hi,
Here are some question about the circuit design of UCC27714:
1. How many MOSFET can UCC27714 drive? If now I want to drive 4 high-side MOSFET, the Ciss=10n, Vbt=11V,
and the driving current will be 1A(4A/4) per MOSFET, so I will know the charging time will be 10n*11V/1A=110ns.
If operating frequency is 300KHz, then 110ns is about 3% duty, not a good design. But the duty will be less than 1% if the frequency is 10KHz, good design.
Am I right?
2. Or is there any better way to know how many MOSFET it can drive?
3. What value of Cboot I should use? At least highier then 4*Qg/Vboot+4*Cgate(noise filter)?
4. What size of Rboot I should use? I know the peak current of Rboot is (VDD-Vf)/Rboot when first time charging, but it's only the peak current for a short time.
How to calculate the average powerloss for risistor size selection?
Could you please hlpe to answer question by question? Thank you very much!
Best Regards,
C.T.