Hello all,
Question1
TPS65911 is supllying 3.3V and 5V based on SWCU187A.
1st 5.0V is supplied after 3.3V is supplied, it has 20ms delay.
Do you have any concerns? Do you have any specification about both timing?
Question2
SWCU187A showed an external hiside-FET is connected to 12V.
What is the minimum voltage that can be supplied to the external FET?
Best Regards.,
Mitsuharu Iwasaki