This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24070: STAT1 / STAT2 LEDs flashing when battery is around 4V

Part Number: BQ24070

Hi,

I am using BQ24070RHLT to controll charging of a 3100 mAh li-ion battery at 1,3A max current. I am using 1uF capacitor at BAT output. If charging starts with battery at around 4V or higher, both STAT1 and STAT2 LED are flashing at around 9 Hz. On the scope connected to BAT pin I observed that voltage is shifting from battery voltage (eg. 3.94V) to 4.16V and back. It seems that the chip is terminating the charging too quickly, and enters battery recharge state right away. Could you help me resolve this?