Part Number: ULN2003A
Other Parts Discussed in Thread: TPL7407LA
Hi team,
According to the datasheet as below, i have three question about this:
1. Is the maximum Ice current for each channel or the total current for 7 channel?
2. if I am about to use 4 channel, and set two of them with 80% duty cycle, and the other two with 30% duty cycle. What's the maximum current for this kind for application?
3. What's the Vs voltage and other test condition for the below picture?
Could you please share some advice for this?
Thanks.