Hi,
I am driving a half bridge with the UCC27201 but have a 5k resistor connected between the HS side FET source and 3.3V and a 220k resistor (a 200k plus 20k resisitive divider) connected between the HS FET source and GND. I need to know the resistance between VCC of the UCC27201 and the switch node (source of HS FET) or the current coming out of the switch node when both HS FET and LS FET are off.
Thanks,
Nick