Other Parts Discussed in Thread: UCC28780,
Hi,
I use UCC24612 with UCC28780 for an adapter design.
In UCC24612 datasheet, it say UCC24612 will use 70% of previous switching cycle.s SR off time as the minimum off time.
In UCC28780 there are ABM mode and LPM mode.
In LPM, there are 2pulses in a burst preriod, so the off time of the second pulse is too long due to enters into burst off time.
So for the new burst mode, the second SR driver signal couldn't be sent out due to the long off time of the first SR driver.
There is the same issue for ABM mode.
It looks it is the inherent issue of UCC24612 when it is cooperation with UCC28780. Right?
BR