I am using BQ24295 chip, encounter the problem of disconnecting VBUS voltage, sys voltage power off. VBUS input voltage is 5V, BAT voltage is 3.9V, sys output voltage is about 4V. There is no use of boost external charging and USB function.I want to know how the two voltages of VBUS and BAT are switched.
1. VBUS Voltage Drop How Much Start Switching Battery Voltage Supply
2. How long will it take for VBUS to switch to battery voltage?
Is it the 30ms mentioned in the screenshot?
3. When VBUS rises, what conditions will be satisfied to switch back to VBUS? Is the switching time the same as the 30ms shown above?
4. The minimum voltage of sys pin is determined by REG01. At present, we have 3.7V on this side and 3.9V on the upper limit of battery voltage charging. How to improve the output voltage of sys? What I understand is that the maximum charge voltage of the battery set (the battery charged to the maximum set voltage) +150 mV. For example, I now upgrade the battery voltage ceiling to 4.2V. When the battery is full, the sys pin output voltage is 4.35V?
thanks a lot.