This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have used LP38692SD-ADJ/NOPB in one of my board but now i want to use a LDO which can source output current greater than 1.2 Amp and voltage 5V with input 6V and should be footprint compatible with LP38692MP-5.0/NOPB that is SOT-223-5 package.
Thanks