This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS259250-61EVM: Minimum UVLO threshold

Guru 19655 points
Part Number: TPS259250-61EVM
Other Parts Discussed in Thread: TPS25942L

Is there way to set Input UVLO less than 4.3V? (Request is 3.8V)

One customer want to set 3.8V ULVO on/off and EN/UVLO pin can set these threshold by R1 and R3, but Vin input UVLO could not set.

⇒Request is Device off: less than 3.8V, but in fact device off: about 4V. 

Best regards,

Satoshi