This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: BIN thermistor function the same as BQ27426

Part Number: BQ27441-G1
Other Parts Discussed in Thread: BQ27426

Hi,

Im looking at using the BQ27441 instead of the BQ27426 in a design.

What I am not clear on is the BIN pin. they have the exact same pin description and it looks like the same function but it is not explicitly stated in the BW27441 datasheet.

The battery thermistor is being used by the charge IC and I want to connect an external thermistor to the BIN pin. The BQ27426 clearly states in section 8.2.3 that it supports an external thermistor, the BQ27441 makes no mention of it.

I believe that they will function the same, the parts are in the same family and have the exact same description on the datasheets and in the reference guide, but I would like someone to confirm this.

Thanks,

Luke