Dear TI:
When I used Webench to design LM3478 schematice, the Webench hint: "With the design conditions, either the IC or the selected FET junction temperature is exceeded above the maximum rating. Hence, this design is created using an ideal FET. Please note that the resulting FET parameters are ideal, so the efficiency/loss opvals have been disabled. Also, the schematic/PCB export and Thermal simulations will not work with the ideal FET."
What does that mean?Does it mean that LM3478 cannot actually meet the design requirements?If it can be satisfied, can you provide a reasonable design device selection?
Thanks!
The design requirement is:
Vin=3.2V-4.2V
Vout= 50V/0.2A