Hi,
I'm currently debugging a new board with the LM5176PWP and unfortunately I see an issue I can't solve. For me it looks like all conditions or voltage levels of pins connected to external circuits seems to be fine but there is no output signal. I see that soft start stays at zero, the low side MOSFETs of the input stage in constantly on, but this condition is stable without any change.
* input voltage is 48V,
* input current is small,
* output voltage nearly zero,
* both current measurements are nearly zero, I'm measuring at the output,
* EN/UVLO is about 1.6V,
* RT constantly 1.25V, there is a 62k resistor to GND
* Mode = 2V, there is a 91k resistor to GND.
* VCC = 7.4V
The voltage at the soft start pin stays low all the time, also during startup. Do you know a reason for this behavior. No MOSFETs are switching in PWM mode, not at startup and not during constantly powered condition, only the low side gate 1 is constantly active.
The datasheet mentioned a short output protection. It's not short but I don't find much information related to this feature.
I found here at E2E a user with more or less the same issue, but unfortunately this post is locked and a can't add my question there. On the other hand, the users initial post explained the same situation, that there is no output although all pins have right signal, but the conversation ends with a discussion about output capacitors...
Maybe somebody have seen the same behavior and can give me an idea where to start with.
Thank you so much,
DH