This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: For better efficiency working with solar panels

Part Number: BQ24650
Other Parts Discussed in Thread: BQ24195

Hello,

Currently in my system I am charging my LiPo batteries from solar panels using BQ24195 which is not specifically designed for solar power charging. Would there be any improvements in the efficiency and charging processes if I used BQ24650 which is designed specifically for solar charging solutions.

Regards,

Prudhvi Sagar

  • Prudhvi,

    The BQ24195 is likely more efficient than the BQ24650 because it is optimized for charging single cell batteries where the BQ24650 is optimized for 2-3 cell batteries but can charge a single cell battery. The BQ24650 has external resistor controlled VINDPM, called MPPSET, which essentially regulates the charger's input voltage to the solar panel's MPP, typically 80% of its open circuit voltage (VOC). The host software can use I2C to set the BQ24195's VINDPM level to the panel's MPP point as well.