This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62740: When Vin<2.2V, TPS62740 does not work, but the resistance between the Vout and GND is 20-30 ohms.

Part Number: TPS62740

TPS62740 Vin Voltage range is 2.2~5.5V

We encounter a problem that when Vin is less than 2.2V, Vout is almost connected to the ground.

Is the resistance between the Vout and the GND very small when the chip is not working?

Is there any explanation from the internal circuit of the chip?Like the Vout Discharge circuit, the internal feedback divider network, etc.

TPS62740 TPS62742 bd_TPS62740_41.gif