HI
I'd like to ask you the below.
*Development product specifications
- 48V/12V 3.5kW DCDC Converter
48V → 12V Buck Mode : 3.5kW
12V → 48V Boost Mode : 1.0kW
- 6 Phase (LM5170-Q1 3ea)
*Questions
1. If I use the Analog Outer Voltage Loop Control, can I apply only one external error Amp to the 6-Phase?
2.Is the Power MOSFET Failure Detection operating only in the initial start-up state or can the MOSFET Short be detected during normal operation?
3.In the figure below, what should be considered in order to determine the TVS Diode capacity used in front of the circuit breaker?
- Apply 3600W TVS Diode in EVM Circuit Diagrams
Thanks