This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478: Sepic mode Component Values

Part Number: LM3478

Hi,

I want to use LM3478 in Sepic mode

Input = 6V to 10VDC

Output = 8V / 3 Amps (If 3 amps cannot be provided, advise the max current that can be provided with 8V as output)

Kindly advise how to calculate the 2 inductors, L1 and L2, output capacitor, Cout, Input capacitor Cin, MOSFET rating and other associated component values

Regards

Atul Bhakay