This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2825: Idea for disable setting

Guru 19655 points
Part Number: UC2825


I need to add disable circuit for UC2825(Push-pull) due to measure abnormal prevention. 

I think that UC2825's CT pin left short by external circuit, UC2825 will be disable. (oscillation will stop)

Is this idea no problem?

If there the other good idea, please let me know. 

Best regards,

Satoshi

  • Hi Satoshi,

    I have asked one of my colleagues to answer this question, but please understand that response may be delayed due to holidays. Thank you.

    Regards,
    Teng
  • Hi Satoshi,
    Normal methods for shutting down the UC2825 are either:
    a) Pull the ILIM/SD pin up above 1.4V.
    b) Pull the Soft Start pin down below 1.1V. This can easily be done using an external transistor or gate fed through a series diode.
    I recommend using the second option since once the fault is cleared this will allow the part to start normally.
    Thanks
    Joe Leisten