This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563219A: Package question

Genius 17335 points
Part Number: TPS563219A

Hello,

 

I have a question for TPS563219ADDFR package information.

 

From the datasheet(SLVSDP9), there is a package outline page, P28.

The below is from the page.

 

In this picture, please see blue and red marked values.

There are “TYP” in blue marked values and there are NOT “TYP” in red marked values.

What is the difference between them and What does this “TYP” mean in this case?

 

Regards.

Oba

  • Hi Oba, 

    An example of length A, it shows 2.95 and 2.85. It indicates the max value is 2.95, and min value is 2.85. And typical value is 2.9. 

    Although it doesn't write "TYP", it actually has a typical value. There is no difference between 'TYP' and 'NOT TYP'. 

    BRs, 

    Edwin.