This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS543C20: MODE pin resistor tolerance

Part Number: TPS543C20

Please let me know the resistor value tolerance of MODE pin.

I understand tolerance of 1% or less are recommended in datasheet.

However our customer used 22.7k ohm though 23.7k ohm have to be used. Is this value allowed?

How much tolerance is allowed for MODE resistor in fact?

We would like to know reference value even if over 1% tolerance is not guaranteed.

Best Regards,
Kohei Sasaki