Other Parts Discussed in Thread: REF3450
LM4030B is a "ultra-precision" shunt reference (1% and 20ppm/°C) up to 30mA.
Is there an (easy) application to build a (ultra-precision) 5V reference with more current capability?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roberto,
What are the exact specifications you are looking for?
It is possible to use a REF3450 with an external FET to achieve 5V with 200mA+ source current.
Any of our series references can be modified with a FET for current boosting.
Follow the directions from figure 7 of this datasheet

-Marcoo