Other Parts Discussed in Thread: PMP9779
Hello,
I have used LM3478 as a boost converter which takes 5V as input and produces 12V @ 3.6A. I want the output current limit to be 4A, so I calculated Rsen as 10milliohm. The inductor value used is 2.2uH and switching frequency is 500Khz. Additional slope compensation resistor (Rsl) of 100 ohm was used along with 10nF capacitor (Csl). I have observed the following:
1) The output is regulated at 12V till 3.8A which is desirable.
2) As 4.5A output load is applied through 2.667 ohm resistor, the voltage drops to 11.6V instead of dropping to near 0 volts. The output current was 4.23 A.
3) As 5.5A output load is applied through 2.2 ohm resistor, the voltage drops to 10.6V instead of dropping to near 0 volts. The output current was 4.78A.
4) As 6A output load is applied through 2 ohm resistor, the voltage drops to 10.2V instead of dropping to near 0 volts. The output current was 5A.
So, is the above behaviour normal? I was expecting the output voltage will drop considerably to almost 0 volts as soon as current limit is exceeded. Is there any error in the design?
Thanks,
Bhargav Saikia.