I have an embedded device where I am thinking about using the TPS23880 device for power distribution. Since the SRAM needs to be loaded each time the device is reset, I need to be able to save the SRAM image in my device's flash memory. Can you tell me the expected maximum size of the SRAM image that I would need to plan for so that I can set that amount of flash aside? I don't seem to be able to find this information in the datasheet.
Thanks.