hi sir,
my customer using TPS62130 for 5v to 4.12v buck application, the IMAX is 2A in their design. now customer find two question, they want to know the reason
1. when the output current from 100mA to 1.8A, they find that the frequency of SW pin will change from 1.38MHZ to 200KHZ, could you please help to check if this is normal ?
2. when the output current is 200mA, They found that the peak to peak voltage of SW pin will rush to 5.6V, This is why, is it normal?