Other Parts Discussed in Thread: LM5170
Hi,
I'm planning to buy this LM5170EVM-BIDIR EVM for my one of the requirements as boost mode only. So kindly help me with my answers in very short form to decide:
1.> My requirement is I/p Volt Entire Range from 12-48DC and O/p is needed to charge 48V battery i.e 50.5V but need 10-11A current, so can i use it? (answer me in yes or no)
2.> Do i need to pile multiple cards for my requirements or only one card? (answer me yes or no)
3.> if above question is yes, how many slave cards i will need? (answer in numbers 1-3)?
4.> Does it have Short Circuit protection? (answer me in yes or no)
5.> Does it require any heatsinks? (answer me in yes or no)
6.> if above question is yes, which model or part number if you can suggest?
7.> How do i know if battery @ O/p is fully charged?
Deeply awaiting your reply.
Regards!