This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMZ14203: 3.3V operation

Part Number: LMZ14203


Tool/software: WEBENCH® Design Tools

In webbench power designer I ma not able to enter 3.3V , 3Aoperation for LMZ14203. It says no value lower than 5V supported. I guess data sheet says 3.3V operation possible.

How get use webbench for LMZ14203 for 3.3V output voltage??

My input supply is 23V- 35V.

  • Hi Rakesh,

    I was able to generate a WEBENCH design for 23V-35V input, 3.3V output at 3A load. Attached is the shared design link. Please take a look and let me know if you see this design. 

    LMZ14203 WEBENCH Design Link: https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=03ABAFF91DBE8820

    Regards,

    Jimmy