Hi Everybody,
i approached to a multi stage converter in several posts.
the last stage is buck converter which should to be controlled with a micro-controller.
the input voltage is 0-400 VDC ( from a half bridge stage ) and the output is 0-400 VDC. the maximum current is 1 A at 400 V and 10 A at short circuit.
the output current should to be controlled through a closed loop.
i have several questions:
1) how can i select between peak and average current mode control?
2) what are the considerations?
Best Regards,
Ras