Other Parts Discussed in Thread: TPS54628
Dear Experts,
Condition: Input 12V, output 3.7V, loading 2.5A
We found high side Vds of TPS54628 will be about 18V.
Is TPS54628 high/low Vds rating the same as 20V (22V<10ns)? Could you help checking voltage rating spec of high side Vds?
If answer is yes, 18V is over our 85% derating guideline.Would you think it will be a risk?